DANGER
HAZARD OF ELECTRIC SHOCK.Remove all power from all devices before removing any covers or doors of the system. Disconnect the power at the device and at the power source.
WARNING
ELECTROSTATIC DISCHARGE REQUIRED.Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.
NOTICE
COMPLEX PROCEDURE REQUIRED.The resolution of this article has many complex steps that may result in unforeseen results if not performed correctly. If you are at all unfamiliar with the requirements, please contact Product Support Services for assistance.
Issue
Where is the encoder card for the Esprit IP located?
Product Line
Pelco Cameras
Environment
- ES40E
- ES41E
Cause
IP Encoder Card location
Resolution
The Esprit IP encoder card is a Non-Field Service recommended performance. The encoder card is seated well within the base of the Esprit IP.
It is recommended to consult with Pelco Technical Support to fully determine a resolution to any operation questions of the Esprit IP
NOTE: Entire Power Base module may be reviewed with technical support for a possible field exchange.