Unable to activate patterns on a Spectra Lite dome drive.

Issue

No option to program a pattern

Product Line

Pelco Cameras

Environment

  • Spectra Lite
  • DD5TAC
  • DD5T-C

Cause

  • Unable to program a pattern from control system
  • No PATTERN text display when attempting to program pattern
  • No menu option of pattern

Resolution

Spectra Lite models did not feature the option to program patterns. A Spectra Lite may be identified by either of two viewing options:

At Power Up
Pelco Spectra Lite
Configure Done

Spectra Lite Main Menu options:
*
Camera
*Line Sync
*Power Up
*Other
  EXIT


Note: If patterns are required, it is recommended to consider the purchase of a new Spectra IV SE series:

  • Patterns: Up to 8, On-Screen, User-Defined Configurable Patterns;
  • Includes Pan, Tilt, Zoom, and Preset Functions.

    Additional functions included for the Spectra IV SE:
    Park Action: Pattern
    Power Up Action: Pattern