How to program a pattern on the Spectra II, Spectra III or Spectra IV using the CM9502-KBD.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How to program a pattern on the Spectra II, Spectra III or Spectra IV using the CM9502-KBD.

Product Line

Pelco Cameras, Pelco Matrix

Environment

  • CM9502 Matrix
  • CM9501 Matrix 
  • CM9502-KBD
  • Spectra II, Spectra III, Spectra IV

Cause

Program a pattern on the Spectra with the CM9502-KBD

Resolution

PROGRAMMING PATTERNS

  1. Call up the camera to the controlling monitor.
  2. Move the camera to the where you would like pattern to begin.
  3. Tap F9 and then tap F1 on the keyboard. On the video monitor screen there will appear text  "PROGRAMMING PATTERN" or "REMAINING STORAGE" to indicate pattern programming has begun.
  4. Move the PTZ through the desired movement pattern
  5. Press F9 and F2 to end pattern programming.
  6. To run the pattern just programmed, press the F5 button while in the "RUN" mode.
  7. Click Here (CM9502-KBD) to view image of keyboard.