Quicktime player will not display a 2048 X 1536 MJPEG view

Issue

Quicktime player will not display video in the 2048 X 1536 MJPEG mode. This is a 3 megapixel mode

Product Line

Pelco Cameras, Pelco Video Management

Environment

3 megapixel camera, quicktime player

Cause

This is a limitation of the quicktime player and the RTP jpeg header in it.

Resolution

There is no resolution other than lowering the resolution or using the Pelco media player