Issue
Badge printing was working, but when trying to print now the error is shown. The Windows user has full admin privileges
Environment
Continuum
EpiBuilder
Windows XP
Windows 7
Windows Server 2003
Windows Server 2008
Cause
Layouts are contained within files and the path can be specifically selected
Resolution
Ensure that the path to the layout is correct
Ensure that the layout is the correct layout.
Test with multiple layouts as it could be one particular layout that is corrupt.