How to set the FS85011 fiber module for coaxitron protocol.

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

No coaxitron control of Spectra III/IV with FS85011.

Product Line

Pelco Cameras

Environment

  • FS85011AMST
  • FS85011ASST
  • FS85011ASFC

Cause

No PTZ coaxitron control from controller

Resolution

  1. Coaxitron: Enabled when the 2-pin header plug (P3) is not connected to the header. If Coaxitron is required, remove the plug from the 2-pin header and attach it to one pin only for later use. (factory default is RS422 setting)
     
  2. Note: FR85011 Series: Ensure the data selection switch is set for Position 5 for coaxitron setting.

     

Vew for the following arcle: How to set the FS85011 fiber module for 422 control