Which substitution codes are available for write to file notification objects?

Issue

Which substitution codes are available for write to file notification objects? Customer wishes to write dynamic values to file.

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation 1.3/1.4

Cause

When using write to file notification objects it may be desirable to have dynamic text containing actual values etc.

Resolution

For write to file notifications, the substitution codes can be used in the message but not in the file name. A substitution code for notifications has the form @([property]) where [property] is replaced by one of the alarm properties. If you use a substitution code that is invalid for the specific alarm event, the substitution code is replaced by an empty string.

Substitution Codes for Notifications can be found by following this link: LL#13539