Reset a Sarix IE series Network Dome Camera to factory default.

Issue

How to reset a Sarix IE Series Network Dome Camera to factory default

Product Line

Pelco Cameras

Environment

Sarix IE Series Network Dome Camera

Cause

  • Forgot password.

  • Resetting ip address

  •    Defaulting

Resolution





IMP Series Mini Dome: 
Default: Using a small tool, such as paper clip, hold down the reset button longer than 5 seconds to reset the camera to factory defaults.
Reset: Press the reset button briefly and release to restart the camera.

 

 

NOTE: The lower dome must be removed to access this button.

  1. Using a small tool, such as a paper clip, press and release the rest button once to reboot the camera.
  2. Press and hold the reset button for 10-15 seconds to restore the camera to the factory default settings.

Side Note: If this reset fails, try to remove power, Hold in reset button and power the camera back on as it powers on continue to hold reset button in for 15 seconds then let go.
 

AFTER RESETTING THE CAMERA, THE IP ADDRESS WILL BECOME THE DEFAULT ADDRESS OF 192.168.0.20 ( UNLESS THAT ADDRESS IS ALREADY TAKEN AT WHICH TIME IT WILL CHOOSE THE NEXT AVAILABLE IP ADDRESS IN THE 192.168.0 NETWORK)