Does the DSSRV support resolutions higher than 1280x1024?

Issue

Does the DSSRV support resolutions higher than 1280x1024?

Product Line

Pelco Monitors, Pelco Video Management

Environment

  • DSSRV - All versions
  • DS
  • PMCL524F

Cause

DSSRV will not allow 1920x1080 as a supported resolution.

Resolution

Yes the DSSRV does support resolutions higher than 1280x1024.

1. Right-click the Intel Graphics and Media Control Panel icon in the system tray and select Graphics Properties.


2. The Intel Graphics and Media Control Panel wizard will launch, click the Control Panel button at the bottom.


3. Go to General Settings and verify that Display shows the correct monitor display.

 4. Under Resolution select the desired resolution.

5. Hit OK to save settings