Which KBD controller's are compatible with the DX Series Video Recorders.

Issue

Would like to use the KBD5000 of the KBD400 with the DX product line.

Is the KBD300A the only KBD that will connect to the DX Product line.

Product Line

Pelco Video Management

Environment

  • DX4000 DVR
  • DX4100 DVR
  • DX4500/DX4600 DVR
  • DX4700/DX4800(HD) HVR
  • DX8100 HVR
  • DX8000 DVR
  • KBD300A
  • KBD5000
  • KBD400

Cause

KBD5000 keyboard compatibility with DX Series Recorders or the DX Series Client software.

Resolution

No. The only keyboard that is compatible with the DX Series Recorder is the KBD300A (version 5.0 or higher).

The DX8100 will require the KBDKIT

The DX4500/DX4600 or DX4700/DX4800(HD) will require the KBD300USBKIT

Note:
The DX4000 and DX4100 are not compatible with the KBD series

Related articles:

How to connect a KBD300A to a DX8000/DX8100 series recorder?

How to connect a KBD300A keyboard to a DX4500/DX4600 Series HVR.

How to connect the KBD300USBKit with the DX4700/DX4800 series DVR.