Add multiple Live tabs in DS ControlPoint.

Issue

How to add new Live tabs in DS ControlPoint when using a single display monitor.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint

Cause

On a single monitor client PC running DS ControlPoint, need Live tabs created to populate all cameras from connected DVR's, then able to click on the different tabs to display a new layout of cameras.

Resolution

  1. Open the DS ControlPoint client software (Start > All Programs > Pelco > DS ControlPoint)
     
  2. Click on the Live icon  at the top left of the screen.
     
  3. Click the Plus button to add a more Live tabs.


     
  4. Click the X to close a Live tab when no longer needed.

 

Information on using with multiple monitors, refer to article: How to create a multiview in DS ControlPoint and undock it to be used on another monitor.