PMCL542BL bezel width.

Issue

  • How wide is the PMCL542BL bezel?
  • The PMCL542BL bezel width is how many inches?
  • What is the width of the bezel on the PMCL542BL monitors?

Product Line

Pelco Monitors

Environment

PMCL542BL monitor ONLY.

Cause

The PMCL500BL series documentation makes no reference to the width of the bezels.

Resolution

The side bezels (left and right bezel widths as looking directly at front of monitor) are measured at 27.7mm or 1.09".

The top and bottom bezels are measured at 28.4mm or 1.118".