Is the KBD4000 compatible with CM6700/CM6800 series?

Issue

KBD4000 Compatible with CM6700/6800?

Product Line

Pelco Matrix

Environment

  • KBD4000
  • CM6800 SERIES
  • CM6700 SERIES

Cause

By design the KBD4000 will work only with Genex Multiplexers and Multiplexer servers in conjunction with Genex Multiplexer.

Resolution

The KBD4000 is not compatible with the CM6700/CM6800 series.

It would be recommended to use a KBD300A.