Spectra I II III IV Series

Issue

Spectra models

Product Line

Pelco Cameras

Environment

  • Spectra I  series
  • Spectra II series
  • Spectra III series
  • Spectra IV series

Cause

How can you tell if you have a spectra 1, 2, 3 or 4

Resolution

If the spectra model number begins with the following.

  • DD5-C / DD5-M / DD5T-C its a Spectra 1
  • DD5AC / DD5BC / DD5TAC / DD5AM  its a Spectra 2
  • DD53TC16 /DD53C22 /DD53CBW its a Spectra 3
  • DD423 /DD427 /DD4CBW18 /DD4CBW35 /DD429 /DD436 its a Spectra 4

Related articles:
Spectra Series Compatibility