Issue
When configure a door with both reader channels as 0, only want to monitor the status of door switch, when the door is opening for a long time, the door ajar alarm should be triggered if the alarm has been configured, but on this condition, the door ajar alarm will never be triggered.
Environment
Cyberstation
ACX
AC-1
Cause
Maybe it is a design, the controller not consider is a door when the reader channel is 0
Resolution
Set a valid channel number for EntryReader although it is not connected, then try again, that should be OK.