Can you Digital Zoom an exported video clip in DS Media Player?

Issue

Enabling Digital Zoom in DS Media Player.

Product Line

Pelco Video Management

Environment

  • Digital Sentry
  • DS ControlPoint
  • DS Media Player
  • IMedia.exe

Cause

The DS Media Player software is able to Digital Zoom, but must be enabled each time that the video clip is opened.

Resolution

Digital Zoom can be used if enabled in DS Media Player.

  1. Click the Options menu and then select Digital Zoom Mode in the drop down menu to enable (verify check mark)




     
  2. A Red HUD (Heads Up Display) displays when Digital Zoom is enabled.




     
  3. Using your mouse pointer, select an area that you would like to Digital Zoom. Once selected then use your mouse wheel to Zoom In or Zoom Out.
    You can also hold down your mouse pointer and move to another area of the frame as well.