What is the part number for the Spectra Anti-Vibration mount adapter?

Issue

What is the part number for the Spectra anti-Vibration mount adapter?

Product Line

Pelco Cameras

Environment

  • SD436 Pendant models
  • SD429 Pendant models
  • SD423 Pendant models
  • SP01-002
  • SP01-003

Cause

Mount Adapter for vibration application.

Resolution

SP01-002    Anti-vibration mount adapter for Spectra IV Series standard and environmental pendant dome systems.

SP01-003    Anti-vibration mount adapter for Spectra IV Series pressurized, heavy duty, stainless steel, and Spectra IV SE Horizon
                      Series pendant dome systems.

                      View I/O manual here for details: Mount Adapter
                      View Specification Sheet here:    Mount Sheet