Are the cabinet keys for the discontinued ACX781 controllers still available for ordering?

Issue

ACX781's are still installed on some older sites but the cabinet keys cannot be found. Can these be replaced?

Product Line

Andover Continuum

Environment

ACX781 Cabinet Enclosure

Cause

No one has the cabinet key and it needs to be replaced.

Resolution

The ACX781 controller has been discontinued since 2007. The stock on the cabinet lock/key assembly has been depleted since then and there are no replacements available.