Modifying the IP address of a Niagara R2 Enterprise Server from Admin Tool does not work.

Issue

New pc hardware was supplied for the server.  A new IP address was configured in Windows.  Tried adding it to the Network Settings tab in Admin Tool.  The numbers added to the fields are not retained.

Product Line

TAC I/A Series

Environment

Niagara R2

Cause

new  pc hardware

Resolution

The IP address entered into Windows is sufficient.  Adding the same information to the Network tab in Admin Tool is NOT required.

Treat the Network tab for a server station as 'read-only'.