EH2508FLIR and EH2512FLIR enclosure information

Issue

Why is the EH2508FLIR or EH2512FLIR not provided with a window.

Product Line

Pelco Cameras

Environment

  • EH2508FLIR
  • EH2512FLIR

Cause

No Window to front of EH2508FLIR or EH2512FLIR

Resolution

It is recommended to view the Pelco lineup of Thermal Imaging here: Pelco Thermal Imaging


The EH2508FLIR and EH2512FLIR does not include a window assembly. The enclosure is designed to be compatible with Flir Optics installation as requested through Flir.

NOTES:

  • EH2508FLIR or EH2512FLIR sold direct to FLIR for package assembly.
  • Sold in a quantity packages of 6 direct to FLIR.
  • Does not include a front window assembly.
  • Hardware Kit. No Labels.
  • View image of product here