What can I do to cut the sun glare on the Spectra Dome?

Issue

What can I do to cut the sun glare on the Spectra Dome?

Product Line

Pelco Cameras

Environment

  • SD436-PB Models
  • SD429-PB Models
  • SD436-PG Models
  • SD429-PG Models

Cause

The installation of the camera is in a place that the sun is causing a glare in the picture.

Resolution

Consider positioning the camera at a different location. A different height of angle may also assist to avoid direct view of highly reflective surfaces.

Review the use of a polarizing filter that may reduce glare. Polarizing Filters are purchased through a local camera shop.