Part number for the Internal Power Supply to the RK5000PS-3U

Issue

What is the part number of Internal Power Supply for RK5000PS-3U?

Product Line

Pelco Video Management, Pelco Transmission & Power

Environment

  • RK5000PS-3U
  • RK5PWR-120

Cause

Power supply failure

Resolution

The part number for the Internal Power supply to the RK5000PS-3U is RK5PWR-120

The RK5PWR-120 is obsolete and can no longer be purchased.  

Part number for the power supply for each FR85011 fiber unit that will now have to be used is PS04-1502-0512 and the 2 pin power connector for the FR85011 fiber unit is CN02-2606-3102G.

View the I/O manual by clicking here.