Where to download Firmware Updates for Sarix IP Cameras and Encoders?

Issue

Where to locate Software / Firmware Update Packages (PPM or ZIP) for Sarix Series IP Cameras or Encoders?

Product Line

Pelco Cameras

Environment

Sarix IP Cameras and Encoders, all models.

Cause

  • Sarix Series IP Cameras/Encoders require software update as part of proper maintenance or issue resolution.
  • Firmware update has been recommended by Pelco Technical Support.

Resolution

The latest Sarix IP Camera and Encoder Software / Firmware Update Packages and Release notes can be found on the Pelco Software/Firmware Download Center link by performing a search for the desired device model number (i.e. IM10DN).
 

Related Articles:
LL#14405 - "How to update Pelco devices using Endura Utilities."
LL#14657
- "How to update Sarix IP Cameras or Encoders using Pelco Device Utility 2.

LL#14950 - "Can Sarix IP Camera or Encoder Software / Firmware be updated from Web Browser User Interface?"