Issue
Which valve actuator is the correct choice for V222?
Environment
V222
7212254000
7212258000
7212262000
7212266000
7212270000
Forta
M22 M50
Cause
Suitable actuators for V222
Resolution
For V222 DN65 to DN100, the Forta series is the recommended actuator.
For V222 DN125 and DN150, M22 or M50 should be used. The Forta series actuator will not fit these valves.