NOTICE
DISCONTINUED PELCO PRODUCT.This product has been discontinued. For further information please visit pelco.com/support/discontinued-products
Issue
"NTLDR" missing error message prompts on the screen with a external storage connected to the DX9200 recorder.
Product Line
Pelco Video Management
Environment
- DX9200 recorder
- DX9200HDDI
- DX8100HDDI
Cause
The BIOS was detecting the SCSI card as the preferred boot device and tried to boot from the external array.
Resolution
Change the boot option.
- Boot DVR into the BIOS menu by Pressing and holding the DEL.
- Go to the Boot menu
- Select "hard disk drives windows.
- Select "1st drive "press enter.
- In the subsequent "options" windows, choose "SATA:PM-ST"
- Select Escape back to main boot menu, then setup boot priority list as usual.