Is there a SmartStruxure specification that includes a piece for Network 8000 migrations?

Issue

Is there a SmartStruxure specification that includes a piece for Network 8000 migrations?

Product Line

TAC I/A Series, SmartStruxure Solution

Environment

Network 8000

Cause

sales request

Resolution

The document is available on the Buildings Business Extranet, under Products > SmartStruxure solution > Sales > Guide Specification.

It's a Word doc so it can be modified to suite the desired needs.

The current version is 1.4 and is available here for convenience.