How do I set up Spectra III to work with VITEK VT-E8 DVR.

Issue

Spectra III full pan control with VITEK VT-E8 DVR

Product Line

Pelco Cameras

Environment

  • Spectra III Series
  • VITEK VT-E8

Cause

Intermittent pan control.

Resolution

  1. VITEK VT-E8 DVR communication through RS485 Pelco- P protocol.
  2. Spectra III must be set to P3/9600 baud.

Note: Ensure to address the Spectra III higher then address 1.