Can the DX8100 be upgraded to a more current version of Windows?

Issue

  • Our DX8100 is on Windows XP and it is no longer supported, can you please tell me if the HVR can be updated to a more current version of Windows?
  • How do upgrade my DX8100's OS from Windows XP?
  • We need to upgrade our DX8100 to a more current version of Windows.

Product Line

Pelco Video Management

Environment

  • DX8100 - All models and all versions
  • Windows XP

Cause

The DX8100 needs to be updated to meet the current site IT network standards.

Resolution

There is no support for upgrading the DX8100 to an unsupported Windows OS (Windows Server, Windows 7, Windows 8, Windows 10 etc). No future development will be made on the DX8100 due to obsolescence.