How do I configure Spectra Series onto Axis Q7401?

NOTICE

POTENTIAL FOR DATA LOSS.
The steps detailed in the resolution of this article may result in a loss of critical data if not performed properly. Before beginning these steps, make sure all important data is backed up in the event of data loss. If you are unsure, please contact Product Support Services prior to attempting the procedure below.

Issue

What protocol should I set Spectra Series to work with Axis Q7401.

Product Line

Pelco Cameras

Environment

  • Spectra I
  • Spectra II
  • Spectra III
  • Spectra IV
  • Axis Q7401
  • Axis Provided Drivers

Cause

Required settings for ptz control of Spectra from Axis Encoder. Required Drivers as provided by Axis. 

Resolution

  1. Set Spectra to Pelco D1/9600
  2. Upload Pelco Driver software onto Q7401
  3. Configure Axis Q7401 for its required parameters.

    Note: Axis Encoder may require Drivers, COMM Port, PTZ Address Configuration. Review the provided axis documentation for further information. Axis drivers are obtained from Axis.com. The site requires a registration. Once logged in, click on support and select the Axis product you are working with.