Issue
After selecting a photo and trying to save it in the Image Enhancement screen, the above error pops up.
Environment
CyberStation 1.94
Cause
Not certain - but possible Windows user profile corruption.
Resolution
Uncheck the resize box under the capture options.
Logged into Windows as another user and the issue was not seen.
The Windows user with the problem was deleted (this was not on a domain) and recreated.