When customizing Personnel attributes, is it possible to change the sort order of the Allowable Attribute Values list in the Personnel Manager?

Issue

The entries are displayed in the order they are entered into the table, is there any way to change the order so that the list of attributes is alphabetical?

Product Line

Andover Continuum

Environment

Continuum Personnel Manager

Cause

The list of Allowable Attribute Values is not sorted alphabetically and is not able to be sorted. The entries will stay in the order they were entered.

Resolution

Unfortunately there is no way to re-sort these attributes into another order. They will need to be removed from the list and then re-entered in the order that they need to be presented.

(Note: Defect#958 has been raised for this issue.)