Where do I land the data wires on the Spectra back box for RS422/485 two wire control?

Issue

Where do I land the data wires on the Spectra 4 back box for RS422 two wire control?

Pin Out

Product Line

Pelco Cameras

Environment

Spectra 4 series

Cause

Do I land the data wires on the RX or the TX of the Spectra 4 for RS422 2 wire control.

Resolution

Data Pin Out

For standard PTZ operation,  all Pelco PTZ cameras require a Two Wire connection.  The data wires connect to RX+ and RX- on the circuit board.

NOTE:  CAT5 or better is recommended for the data wires.


 

Related Topics:

Where do I land the Video Cable on a Spectra PTZ Camera