How to Remote Connect A KBD4000 to the Genex Series Multiplexer

Issue

Connecting the KBD4000 beyond the supplied 25 foot straight cable.

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • MX4016CD
  • MX4009CD
  • KBD4000
  • KBDKIT

Cause

Location of KBD4000 is beyond the distance of 25 ft.

Resolution

REMOTE KEYBOARD CONNECTION

You must order a KBDKIT for the KBD4000. The KBDKIT is provided with a wall block transformer and two RJ45 wall blocks.The keyboard
receives power from the transformer. The RJ45 blocks provide connection points for remote wiring.