Issue
PIMS are going offline intermittently, so that the doors won't unlock
Environment
Continuum
Windows XP
Windows 7
Windows Server 2003
Windows Server 2008
Cause
If doors 1-8 are addressed on one PIM and also 1-8 (even though they are different doors) are addressed on another PIM they will conflict with each other
Resolution
The PIM configuration specifies that Doors 1-16 are addressed on one PIM and 17-32 be addressed on another PIM