Esprit series camera deflection values.

Issue

  • What is the maximum deflection of the Esprit series cameras?
  • What is the maximum oscillation in either degrees (°) per second or inches per second that an Esprit series camera can handle?

Product Line

Pelco Cameras

Environment

Esprit series cameras - ALL models and all versions (ES30/ES31/ES40/ES41/ES40E/ES41E)

Cause

No outwardly facing reference to the value for the maximum deflection.

Resolution

The Esprit series cameras will tolerate a maximum of 1° deflection at an oscillation of 10Hz.