Implicit logs stop working.

Issue

After changing the engineering and electric scale with the spreadsheet the implicit logs stopped working

Product Line

SmartStruxure Solution

Environment

StruxureWare version 1.3

Cause

It is not possible to recreate this problem in version 1.3 SP1.

Resolution

Upgrade to version 1.3 SP1 will solve the problem.