Pelco RJ-45 KBDKIT pinout

Issue

What is the Pinout for RJ-45 KBDKIT

Product Line

Other, Pelco Cameras

Environment

KBDKIT

Cause

Pinout for KBDKIT

Resolution

Below is a picture of the RJ-45 KBDKIT to show its Pinout
 

Parts in KBDKIT:

RJ-45 Wall block: CN14-0380-1200

12 VAC Transformer TRF112.0S.20

 

View Lessons Learned article LL#11233 for "wiring connections when using a RJ31X or third party wall block"