Issue
Characteristics may be necessary for some applications.
Environment
SLO320 006920640
SLR320 006920630
Cause
Output characteristics not defined in documentation
Resolution
SLO320 / SLR320 has 2 light ranges selectable by jumper: 400 Lux and 20 Kilo Lux.
Depending on output this means:
400 Lux - 0-10V - 0 V = 0 Lux, 5 V = 200 Lux, 10 V = 400 Lux
- 4…20mA- 4mA=0 Lux,12mA=200 Lux, 20mA=400 Lux
20 Kilo Lux - 0-10V - 0 V =0 klx, 5 V =10 klx, 10 V =20 klx
- 4…20mA 4mA=0 klx, 12mA=10 klx, 20mA =20 klx