How do you change the FPS (IPS) on a DSSRV.

Issue

Changes FPS on a DSSRV with analog camera attached.

Product Line

Pelco Video Management

Environment

  • DSSVR
  • ENC5416
  • Analog

Cause

The FPS were set too low on each analog camera attached to the DSSRV. 

Resolution

  1. Open DS Admin.
  2. Navigate to the VAU folder.
  3. Open the VAU system name.
  4. Open the Camera folder.


     
  5. Open the Analog H264 Cameras folder to make a globe change to the FPS or Select Individual camera to manually change each FPS. 

For ip camera:

  1. Select the general Tab for ip camera
  2. Select "Edit IP Camera Setting" button.


     
  3. Enter value in the Frame Rate (Image per minute) field.

 

Related articles:
DS ControlPoint plays video back at high speed - fastforward.