What may happen if the same IP address is used by more than one NPR?

Issue

What may happen if the same IP address is used by more than one NPR?

Product Line

TAC I/NET

Environment

I/NET site

Cause

What may happen if the same IP address is used by more than one NPR?

Resolution

A duplicate IP address will cause a system error message in I/NET, and the NPR will not initiate the appropriate LED error code. (TCON 209, 2-27)