APC Xdriver modbus integration information for Continuum

Issue

Information is needed to set up the APC Xdriver modbus UPS integration with Continuum

Product Line

Andover Continuum

Environment

Continuum

Windows XP 

Windows 7

Windows Server 2003

Windows Server 2008

Cause

There are a number of APC devices that support modbus and information is needed to get values into Continuum

Resolution

The following document is provided as an example and will not address every type of APC device.

Download document here

See the following Lessons Learned article for helpful information on bring in modbus values:

Helpful Modbus register Information