Issue
After successfully logging on to the webclient server, there are no contents displayed under root. When clicking the "show contents" button on the top-right of the left pane, a prompt says, "There is no contents can be displayed in this container."
Environment
- Webclient
- Windows 7
- IIS 7.0
Cause
IIS directory browsing feature is disabled for some unknown reason or wrong configuration.
Resolution
- Go to Internet information server manager, click "sites" then "Default website"
- Double Click "Directory Browsing" logo
- On the right "Action" pane, click "Enable", you will see it change to "disable" that indicates the Directory Browsing feature has been change to enabled
- Save and close IIS manager
- Try to log on again.