Issue
The maximum number of backups in Vista is 20, is this possible to change?
Environment
TAC Vista 5.1.8
Cause
When backups in Vista is set up you can specify the maximum number of backups which should be crated before the oldest is overwritten.
Default is two and maximum is twenty.
Resolution
This is not possible to change this is a hardcoded number in Vista.