How to change the Domain/Groups/Administrators setup

Issue

How to change the Domain/Groups/Administrators setup

Product Line

SmartStruxure Solution

Environment

SmartStruxure

Cause

Domain/Groups/Administrators setup is grayed out and thus cannot be modified

Resolution

Domain/Groups/Administrators setup is grayed out and cannot be modified, this is to avoid major changes being made the Administrators Group such that everyone could be locked out of the system.

This can be seen on the following screens

 
 

 
 

 

To change the Users or Workspaces within the Administrator Groups, go to Users or Workspaces modify the Group Membership here