How to create and call a preset on a Spectra HD series Pan Tilt Zoom (PTZ)

Issue

Configure preset positions on Spectra HD network camera.

Product Line

Pelco Cameras

Environment

  • S5118-FW0
  • S5220-FW0
  • S5230-FW0
  • S5118-FW1
  • S5220-FW1
  • S5220-FW1
  • S5118-YB0
  • S5220-YB0
  • S5230-FW1
  • S5118-YB1
  • S5220-YB1
  • S5220-YB0
  • S5118-PG0
  • S5220-PG0
  • S5230-YB0
  • S5118-PG1
  • S5220-PG1
  • S5220-YB1
  • S5118-PB0
  • S5220-PB0
  • S5230-YB1
  • S5118-PB1
  • S5220-PB1
  • S5220-PG0
  • S5118-EG0
  • S5220-EG0
  • S5230-PG0
  • S5118-EG1
  • S5220-EG1
  • S5220-PG1
  • D5118
  • D5220
  • S5230-PG1
  • B5
  • B52
  • S5230-PB0
   
  • S5220-PB1
   
  • S5230-PB1
   
  • S5220-EG0
   
  • S5230-EG0
   
  • S5220-EG1
   
  • S5230-EG1
   
  • S5220-ESG0
   
  • S5230-ESG0
   
  • S5220-ESG1
   
  • S5230-ESG1
   
  • D5230

Cause

Camera Programming

Resolution

To Program the Spectra HD using a web browser; login, click on settings, and choose Presets from the Imaging Tab.

CREATE A PRESET

  1. Enter the name of the preset position.
  2. Navigate to the position using the PTZ control border on the mini video window.
  3. Save.

 

 

CALL A PRESET

Click on LIVE to enter the live view video window. Notice to the left; the PTZ controls.

  1. Click on the down arrow in the PRESET FIELD and a list of created presets will be offered.
  2. Click on the desired preset position

*Note*  The Preset Position may not immediately come up; Select the Preset repeatedly until the position is achieved.