How do you create/delete a user account on a DX4500/4600?

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

How do you create/delete a user account on a DX4500/4600?

Product Line

Pelco Video Management

Environment

  • DX4500
  • DX4600

Cause

System information.

Resolution

Creating a user account:

  • To add create user account on a DX4500/DX4600 click here.

Deleting a user account:

  • To delete a user account. 

        1. Login to the DX45/4600.
        2. Click on the setup icon (cog wheel).
        3. Click on System.
        4. Click on User.
        5. Highlight the user that needs to be deleted.
        6. Click on Delete at the bottom left of the screen.
        7. Click OK on the prompt that comes up.