How do I change the camera names on the CM6700 with the KBD300A?

Issue

How do I change the camera names on the CM6700 with the KBD300A?

Product Line

Pelco Matrix

Environment

KBD300A

CM6700

Cause

I cannot change the characters of the camera name on the CM6700 programming menu?

Resolution

To change the characters on the CM6700 using the KBD300A, use the following sequence of buttons: