How do I wire the ERD2200 for power.

Issue

The Installation/Operation manual is not intuitive for wiring the ERD2200 for power.

Product Line

Pelco Transmission & Power

Environment

  • ERD2200

Cause

  • Installation

Resolution

115/230 VAC Wiring.

To connect the 115/230 VAC input to the receiver:

  1. Remove the cover and land the wire on the power terminals.
  2. Be sure the Power selector switch is in the 115/230 position for 115/230 VAC Pan Tilts.
  3. If there are any peripheral 115/230 devices; land the out put wires on the output terminals.
  4. 24 VAC cameras outputs will land on the 24 VAC output terminal.

 

24 VAC Wiring.

To connect the 24 VAC input to the receiver:

  1. Wire and land the 24 VAC input to the rear of the ERD2200 module.
  2. Land the wires on the 24 VAC INPUT POWER power block.
  3. Be sure the Power selector switch is in the 24 VAC position for 24 VAC Pan Tilts.

 

 

NOTE: The ERD2200 is set at the factory for 115/220 operation.  You will need to take off the label by the power plug and change to 24VAC before the ERD2200 will work with 24VAC