IS50DNV10 and IS50-CHV10 switch settings

Issue

Switch Settings of Day/Night or Color Camera

Product Line

Pelco Cameras

Environment

  • IS50-DNV10 models
  • IS51-CHV10 models
  • IS20-DNV10 models
  • IS21-CHV10 models

Cause

Switch operation for Video Adjustment

Resolution

The Camclosure 2 Day/Night and Color camera models feature a four position dip switch configuration option. The switch modes
are used to adjust the following settings: Turns ON/OFF the day/night mode, adaptive black stretch, backlight compensation,
and white balance.

                                 

View the following pages by clicking here for: Switch Settings