DX8100HDDI Storage System hard drive replacement part number.

Issue

Drive 3 reporting a failure after the rebuild process.

Product Line

Pelco Video Management

Environment

  • DX8100HDDI-6TB
  • DX8100HDDI-12TB
  • DX8100HDDI-18TB
  • DX8100HDDI-24TB
  • RAID 5
  • HDD2K-8100HDDI
  • EonStor

Cause

The DX8100HDDI is running a little sluggish when being accessed. Hard drive failure.

Resolution

2TB Replacement Hard Drive = HDD2K-8100HDDI (EE11-0002-2112)

Note: May require a RAM upgrade depending on age of the DX8100HDDI


DX8100HDDI drive bay order:


 

Related Articles:
Locate the installed DDR RAM size for the DX8100HDDI Storage System
Installing the 1GB Memory module into the DX8100HDDI chassis